Other Parts Discussed in Thread: MSP430FG4619
Hi all,
This is the setup

The MSP430(System controller) is the master and communicates on SPI with UART on MAX3111E .
MSP430 is the master and I am using 3 wire mode with CS to control SPI commn.
The flow of the communication is like this
CS low
Write to MAX3111E configuration register (16 bit) - to set the baud rate etc
CS high
CS low
Read the configuration register to see if the configuration is done properly
CS hi
But I am not able to configure the MAX3111E properly. The configuration is not happening properly (I am writing #CC 0Ch but reading #40 40h).
I think communication is not getting setup properly.
I wanted to confirm two things
1) Do I have to setup the baud rate of UART as per the SPI SCLK(using SMCLK-32768*32 Hz.
2) Also, after sending the command for read configuration register do I have to send dummy bytes to receive data.
3) Do I have to monitor UCBUSY to see if any activity is happening on SPI before deasserting CS. Currently I am using UCA0TXIFG and UCA0RXIFG .
I am attaching the code and also 1882.MAX3110E-MAX3111E(RF LINK).pdfthe datasheet of MAX3111E.
Thanks........