Part Number: MSP430F435
Tool/software:
HI,
I'm currently using an IAR workbench for MSP430. I have a simple project and trying to link a library file with .a extension. also gave a header file for the same. But when calling the function defined in Library, IAR workbench is throwing an error saying the function call is of undefined reference. The same library I'm able to use/link with gcc. I tried with both C based library build on GCC and external C library call built on Rust.
Can we link any external static library file to IAR workbench to call the external libraries? If so what would be the procedure? I don't find any helpful topics or info regarding this from forums or documents available.
Thanks & Regards,
Pranoop.