This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: Problems of connecting to USS. Show "No connected to HID devices".

Part Number: EVM430-FR6043


Tool/software:

Dear Sir/Madam,

I am testing two boards of EVM430-FR6043. One is OK. The other has some problems of connecting to USS.

Sometimes the connecting is OK. But it would be disconnected after one or two minutes. Below is the print screen information of the USS GUI and hardware management of the USB interface.

Below is the print screen information of the USS GUI and hardware management of the USB interface when the board can be connected. 

Could you please provide some information or suggestions for the problems? Look forward to you reply. Thanks!

Jimmy

**Attention** This is a public forum