This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969: Elprotronics FlashPro430 and TI CCS v12

Part Number: MSP430FR5969


Tool/software:

I am trying to set up my development environment with Elprotronics FlashPro430. The FlashPro430 is not detected by CCS out of the box and requires some files (dll and one or two more) copied into CCS installation folder. After following instructions from Elprotronics, I get a message that states "Error initializing emulator: Error loading C:\ti\ccs1260\ccs\ccs_base\DebugServer\drivers\msp430-fpa: %1 is not a valid Win32 application.", which is a 32-bit / 64-bit difference error. Unfortunately, I was unable to find any further instructions in Elprotronics documents. There are 10-year-old threads in this forum with the same problem, but closed with Elprotronics contacting the inquirer and providing or promising to provide an updated 64-bit dll as stated by the inquirer in the forum. I would be happy if anyone here can let me know, if it is possible to use the Elprotronics FlashPro430 with TI CCS v12 and how, since Elprotronic does not reply to my e-mails to them.

**Attention** This is a public forum