Part Number: EVM430-FR6047
Other Parts Discussed in Thread: MSP-FET
Tool/software:
Hello TI experts,
here are a few questions about calibration and hardware design, Please kindly Point us out
Since there are many questions, can you help make an appointment for a meeting and focus on communication?
Calibration:'
The following is the current data collection, calibration and test data on the standard calibration bench, there are still some gaps after calibration, and we need to ask TI experts to help guide us to see where we have not operated correctly, and how to do R400, Q2 0.0001L/H
- Below are our data before and after calibration
校准前 校准后
2The calibration points are set as follows: 16 flow points, Q4, 4500L/h, Q3, 2000L/h, Q2, Q1, and 5 points are set between Q1 and 0.001
3.This is EVM board value:
2024-09-27 17:51:44.286: insert into bp_collect_data values(NULL, 239.651291, 0.570252, 0.570523, 183.198624, 183.198624, 2.896707, 0.000000, 0.000000, 0.000000, 1727430704283, 30.110001, 0.000000, 0.000000, 0.000000, 0.301000, 0.000000, 30.110001, 0.307000, 0.200000, 0.000000, 0.000000, 0.000000, 100.000000);
This is the value of the standard station
表位=9|表号=0.00|流量点=q2000|流量=0.2|标准流量=0.20000|标准体积=0.0335|误差=-100.00|温度1=30.11|温度2=0.00|温度3=0.00|温度4=0.00|压力1=0.301|压力2=0.000|压力3=30.110|压力4=0.307|流量计瞬时流量=0.00000|流量计平均流量=0.00000;
This is the measurement of the USS after calibration, and after selecting the calibration from VFR, it seems to be stable, but it is quite different from the actual flow rate of the standard equipment
HW:
- For actual water meter products, is it possible to convert JTAG and I2C to USB, and use the adapter board to realize it, instead of designing the USB HUB to the board
2.Can I use the general-purpose JTAG programmer used by other MCUs, or can TI MSP430-RF6047 only use MSP430F5528IRGCR to achieve USB to JTAG
3..What is the function of this circuit, what are the benefits of having this circuit, and what background requirements are needed
4.slar139aWhat kind of tool software is used to open the reference file in this?
- Device packaging: Is there a package for MSP430-RF6047 and other devices based on PADS or AD?
- After we complete the schematic design, can TI experts help arrange the review and guidance?