Part Number: MSP430FR2355
Tool/software:
I wrote a quick-and-dirty program for my MSP430 LaunchPad to test if a sensor would detect a magnet but I'm having trouble debugging it because CCS keeps moving the breakpoint I put inside an if statement. Relevant section of code:
// Configure ports
P1DIR |= BIT0; // Config P1.0 (LED1) as output
P1OUT &= ~BIT0; // Clear LED1 to start
P1DIR &= ~BIT5; // Config P1.5 input
P1REN |= BIT5; // Enable resistor
P1OUT |= BIT5; // Make pull-up resistor
PM5CTL0 &= ~LOCKLPM5;
while (1) {
if (P1IN & BIT5 == 0) {
P1OUT |= BIT0;
}
else P1OUT &= ~BIT0;
}
I've tried several different permutations of trying to get the breakpoint to be inside the if statement, but it keeps jumping to the else statement for no apparent reason.