This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-CAPMINI: Firmware binary for CapTivate HID bridge controller (MSP430F5510IRGZT) on EVM430-CAPMINI evaluation Module

Part Number: EVM430-CAPMINI
Other Parts Discussed in Thread: MSP430FR2512, , UNIFLASH

Tool/software:

I am trying to replicate the Captivate HID bridge (MSP430F5510IRGZT) adaptor part of the EVM430-CAPMINI touch evaluation module. It would be a great help if you could provide me with the firmware binary for the HID bridge controller used on the EVM430-CAPMINI board. The circuit for my HID adaptor is a clone of the HID bridge provided on the EVM430-CAPMINI module, so the production firmware binary used on the EVM430-CAPMINI evaluation module should work fine (See attached Schematic). This bridge module is for interfacing our CapTivate touch circuit based on MSP430FR2512 to the TI's CaptivateDesignCenter Application for calibration and testing.

Update:

Finally, I got a chance to test the provided firmware. When trying to flash the firmware for the MCU(MSP430F5510IRGZT) using MSP-Gang programmer, I am getting the following warning and error,

ERROR 396: WARNING: Code from file is out of range in selected MCU

ERROR 386: Code out of range of the selected MCU.

Please find the gang programmer setting below,

I am wondering if the provided firmware TI_MSP_HIDBRIDGE__1_00_03_00__CAPTIVATE-PGMR.txt is suitable for this MCU. It would be a great help if someone can help me in solving this issue.

Thanks,

Thomas

**Attention** This is a public forum