This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: MSP430-RF6047 download and minimum working unit

Part Number: MSP430FR6047


Tool/software:

       Thanks to the support of TI experts, our project has completed part of the hardware test, application software development and algorithm calibration,

and the calibrated measurement accuracy has exceeded the customer's expectations.


      We are preparing the certified machine for the customer, and the current problems are:


60% of the PCBA of the first patch cannot be downloaded and needs to be repaired, and it is currently necessary to understand:

MSP430-FR6047 needs to meet the download conditions, which functional modules are required to be normally patched, and can be downloaded normally?

      That is, if the power supply connection of MSP430 is normal, TEST, RST, 3.3V, and GND are normal, is it possible to download in principle,

or does it still need CLK to work, so it can be downloaded, or does it need other modules to download normally

    Best Regards!

    Larry li

**Attention** This is a public forum