Other Parts Discussed in Thread: MSP430F235
Tool/software:
Hello,
I have to flash a MSP430F235 device on a PCBA, in a production environment. I have to use MSP-GANG programmer. The programmer has to be integrated into a test equipment. I want to connect the PCBA to the programmer trough testpoints, and I want to minimalise the necessary wires. According to my understanding, the MSP430F235 can be connected via JTAG, which require 4 wires (TDI, TDO, TMS, TCK). And of course Power and GND. In the MSP-GANG 14 pole connector there are more pins.:
* BSL-RX and BSL-TX I thnik I can leave them unconnected, please confirm
* TEST pin: the MSP430F235 has no dedicated TEST pin. Should I leave it unconnected?
* nRST pin: if I use JTAG, can I leave it unconnected?
Is there any CLI (command line interface) to execute a script easy, or only the dll is available?
Thanks.
Janos