Part Number: MSP430FR5043
Other Parts Discussed in Thread: MSP-FET, EVM430-FR6043
Tools/Software:
First, here's where the problem starts:
MSP430: Emulator initialization error: One of the connected MSP-FET/eZ-FET debuggers needs to be repaired. Select 'Repair' to start the repair process. Note: Only one MSP-FET/eZ-FET debugger can be connected to the system during the repair process. MSP430: Error: MSP-FET/eZ-FET repair failed
To solve the above problem I bought a new MSP-FET programmer and went through the process again but the problem is still the same.
Initially I was using version 11.0.0.00012 but it is no longer supported so I tried to flash it again to version 12.8.1 and got the following problem:
When I clicked on Detect My Board in View -> Resource Explorer, I got the following error message:
{"msg":"HID_FET: Could not retrieve FET HW version on ( 0: Internal error).","name":"HID_FET","type":"error"}
I read and tried the suggestion to run Program MSP430 (example).bat in another thread, but I still have the same problem.
It seems like the board is not detected because the initial problem was not solved. Is there a way to fix this?
Thanks