Part Number: MSPBSL
Other Parts Discussed in Thread: MSP432E401Y, UNIFLASH, MSP-EXP432E401Y
Tool/software:
Hello Team,
We tried to flash the MSP432E401Y via Ethernet using BSL Scripter.
Following the procedure mentioned in the resource explorer, we have connected a RJ45 Cable from PC, another cable from MCU, and one RJ45 cable from our company's network.
(Actually my previous thread was closed, so starting a new one)
Couldn't flash the bootloader like mentioned in the resource explorer. So we tried to flash the same bootloader with UNIFLASH and did a power reset. Then we could see BOOTP request from Microcontroller in wireshark as below.
When we tried running the BSL-Scripter.exe, its waiting for BOOTP request. Also attaching the BSL-Scripter log file for your reference.
We have quiet alot of unknowns in this, please do answer the following questions.
1. The microcontroller will send the BOOTP request and then the BSL Scripter will send a BOOTP reply with the IP configured in the script as IP Client. and then the updatehandler will update firmware image sent from the BSL Scripter. Please confirm if this understanding is right.
2. Which IP does the BSL Scripter take? The IP mentioned as IP Server in the script.
3. We also tried modifying both inbound and outbound firewall settings for this,but there is no change in the wireshark. only request from MCU is there.
4.
Actually in our application we cannot access the MCU any way except Ethernet. USB is also not possible. In that case, how to erase the Main flash with ethernet,
5. What is the need for connecting the server to the network switch? Is it mandatory?
6. If this is not possible, can you please tell if there's any other way to flash the MSP432E401Y controller via Ethernet?
Thanks in advance.