This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6989: MSP430FR6989

Part Number: MSP430FR6989
Other Parts Discussed in Thread: ENERGYTRACE,

Tool/software:

Dear all,

I'm using MSP430FR6989 launchpad and trying on ultra low power application. Currently, my approach is using LPM45 sleep mode. I assume that with LPM45, the power consumption must around micro ampe. However, my result is around 1.2 mA (measure by EnergyTrace++). Is my problem is from the board itself, or due to my code. My launchpad does not connect to any circuit or components. My code is presented below:

#include <msp430.h>
void enterLPM45();
int main(void) {
    WDTCTL = WDTPW | WDTHOLD;  // Stop watchdog timer
    enterLPM45();          // Enter low power mode
}



// Enter LPM4.5 (Low Power Mode)
void enterLPM45() {
    PMMCTL0_H = PMMPW_H;
    PMMCTL0_L |= PMMREGOFF;      // Shut down power regulator 

    __bis_SR_register(LPM4_bits|GIE);  // Enter LPM4.5 (without GIE)


}

**Attention** This is a public forum