This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: EVM430-FR6047: Water Flow Demo

Part Number: EVM430-FR6047


Tool/software:

Hi all !

I am trying to find the demo firmware from EVM430-FR6047 evaluation board which is the ultrasonic water flow demo. On some forums it's mentionned that the demo is available on USS packages with some code samples but it seems that the firmware is not present anymore.

Also the CCS project of this demo is not available too. Only a minimalist version of the project is available under USS_02_40_00_00\USS\examples\USSSWLib_template_example\CCS. I would like to continue to use USS design center to evaluate TI solutions.

Is there someone who knows where to find the demo binary and even better the corresponding CCS project with all the features exposed inside this demo ?

Best regards.

Loïc

**Attention** This is a public forum