This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969: worst case timing of internal oscillator?

Part Number: MSP430FR5969


Tool/software:

Team, working with a customer on this device. Looking for worst case timing for the conditions below:

PN: MSP430FR5969IRGZT

Temperature: -40 to 63 deg

Storage Life of the part: 30 years

Operational life: 60mins

Let me know if you need any other parameters

 

We are running the internal oscillator for 300ms then switching to the external oscillator for more precise timing.

 

Min

Typ

Max

Tolerance

Units

Timer C (Int Clk)

TBD

0.300

TBD

 

sec

Timer C (Ext Clk)

 

 

 

 

sec

**Attention** This is a public forum