Other Parts Discussed in Thread: CC2560, CC2500
Hi,
I am about to start a project of lighting control project via bluetooth with microcontroller, but I have difficulty in choosing which microcotroller.
So, could anyone kindly tell me that what is the difference between the microcontroller 8051 and msp 430? Which one is more suitable for developing a simple light controlling system, as in which of it can be used to receive signal from bluetooth devices and control the brightness of lights as well? Or is there any bettter idea of which microcontroller that i can use?
MSP430+CC2560 should be good enough for this project right? But the price is a bit too expensive for us. so is there any other microcontroller + bluetooth module can take place of it? since the project is quite simple.
Thanks in advance.
BR
Ivy