Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG,
ti_msp_dl_config.h ti_msp_dl_config.c
Hi,
I am using CCS21 and sysconfig_1.28.1 and mspm0_sdk_2_11_00_07 and the MSPM0G3507
When I compile the code the follow error is consistently generated in the "ti_msp_dl_config.c" file generated by the SysConfig file "basic_node.syscfg" (files attached)
Arm Compiler: "ti_msp_dl_config.c"
[10]ti_msp_dl_config.c:213:9: warning: call to undeclared function 'DL_SYSCTL_enableSYSPLL'; ISO C99 and later do not support implicit function declarations [-Wimplicit-function-declaration]
213 | DL_SYSCTL_enableSYSPLL();
| ^
1 warning generated
The error is in the function "SYSCONFIG_WEAK void SYSCFG_DL_SYSCTL_init(void)" copied below.
The DL_SYSCTL_disableSYSPLL(); does not error
I tried adding the include directly with no effect.
Can someone point me in the right direction to correct this issue?
Thanks,
Mike