Other Parts Discussed in Thread: MSP430F1101A
MSP430F1101A
I would like to set almost all of the 16 interrupt vectors to point to one function, but I dont want to do 16 of:
interrupt [n] void isr_n(void)
{
}
where "n" is the vector offset..because i dont have enough room for 16 functions to be defined in ROM..and I want to make as little of a foot print as possible because this is for debug..
id like just one function that gets pointed to by every vector in the table. (with the exception of maybe 1 or 2 vectors)
im guessing some kind of .iseg statement in assembler, but AQ430 tells me not do mess with that...
cant I command the compiler to just put bytes in the vector table somehow?