This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm developing an application based on the Solar Energy Harvester Code (eZ430-RF2500-SEH) and I'm having a lot of trouble with it. The receiver and transmitter often do not establish a link and so the receiver goes into permanent sleep mode. I have to reboot it (by cycling power) to even try again and it usually does not work. From looking at TI documents it seems like the problem is with the receiver/computer connection via USB. The only thing that works (and it only works sometime) is to reboot the computer and then plug in the receiver. Sometimes this will work and then I can receive data from the transmitter board. Even when it does work I often have to cycle the power on the transmitter in order to get it going - i.e. it does not work on the first power up but works on the second, and on any subsequent cycles. Another thing I notice a lot is that when I power up the transmitter, the Access Node bubble on the PC software will hang (stop updating) for several seconds and then start updating again.
I'm curious if anyone else has seen this behavior, and if so does anyone know how to fix it.
I have tried both versions of the firmware - my devices shipped with 1.3 but I have downloaded 1.5 from the TI site.
It's quite painful because I am making frequent code changes (10+ /hour) and each time I reprogram the device I have to pray that it will communicate with the receiver when I power it up. So any advice will be greatly appreciated. Thanks!
-Chris
One item of note, the antenna design on the ez430-RF2500 is not very efficient. That is why I removed the chip antenna and replaced it with a UFL connector so that I can put a whip antenna on my RF2500 boards. For one thing I don't think they have enough ground plane for the chip antenna on the board. The highest RSSI I have seen on a stock RF2500 board is about -80 with 1 foot spacing between two RF2500 boards.
Falingtrea, how did you take off the antenna? did you use a regular soldering iron?
**Attention** This is a public forum