Other Parts Discussed in Thread: MSP430FG4618
I'm attempting to migrate some code from an MSP430FG4618 over to an F2618 and one of the problems I'm encountering is that I can't figure out how to configure the load capacitors.
I started with some example code, which used the following code:
FLL_CTL0 |= XCAP14PF; // Configure load cap
However, all the documentation I've found on XCAPxPF indicates its only 2 bits
XCAPxPF Bits 5−4
Oscillator capacitor selection. These bits select the effective capacitance
seen by the LFXT1 crystal or resonator. Should be set to 00 if the
high-frequency mode is selected for LFXT1 with XTS_FLL = 1.
00 ~1 pF
01 ~6 pF
10 ~8 pF
11 ~10 pF
Could someone explain how I configure the load capacitor and how I tell what its set to?