This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The USCI_B0 I2C subsystem uses the same interrupt vector USCIAB0RX_VECTOR for both the RX data and bus-status change.
Operating as a slave device:
- Ray
No. In I2C mode, RX vector handles the status change and TX vector handles both, RX and TX. However, the IFG bits keep their meaning:Raymond Dunn said:The USCI_B0 I2C subsystem uses the same interrupt vector USCIAB0RX_VECTOR for both the RX data and bus-status change.
"There are two interrupt vectors for the USCI module in I2C mode. One interrupt vector is associated with the transmit and receive interrupt flags. The other interrupt vector is associated with the four state change interrupt flags. Each interrupt flag has its own interrupt enable bit."
Sadly, this text doesn't tell which is which.
As with all other interrupts except for the ADC10 and Timer-CCR0 interrupt, you'll have to clear teh IFG bit that caused the interrupt, either manually, or by readign the IV register (if available) or removing the interrupt cause (e.g. writing to TXBUF, reading RXBUF). Some may auto-reset. Like UCNACKIFG and UCSTPIFG are cleared by an incoming start condition etc. But if you're already inside the ISR, you might be confused. On 5x family, there is only one interrutp vector for all USCI events, and it has an IV register, that tells you which interrupt is pending and at the same time clears the IFG bit. However, in case of I2C, its use is not recommended, since clearing the RXIFG bit also releases the I2C state machine and you might experience an immediate RX overflow :( So unless you know that you stil have enough time to read RXBUF (1 I2C clock cycle) after reading the IV register...Raymond Dunn said:when processing the bus-status change, is there any flag that needs to be acknowledged to satisfy the interrupt?
Raymond Dunn said:is is possible for data RX and bus state change to occur simultaneously?
Sicne they are in two different ISRs... However, it might be a good idea that in receiving a stop condition or (re)start condition interrupt, you should check for any leftover data in the RXBUF that might just have arrived. (I don't know off-hand which interrupt has priority on 2x devices) before you do anything that might drop it.Raymond Dunn said:should USCIAB0RX_VECTOR interrupt processing check for RX or bus-status change first (one has priority over the other)
Thanks for THAT one!
I was banging my head trying to track down why I was getting unexplained TX interrupts on the slave. I moved the interrupt processing triggers around, and it works correctly now.
I re-read the sections on I2C interrupts in the datasheet, and even knowing the correct interpretation now, I'm not sure I understand what it said. Please have the tech writers review that, and come up with a better explanation. Even the examples shown were confusing. I'm sure having fits understanding several things in the TI datasheets.
I'll do some more extensive testing soon, but the slave works in the nominal cases I've tested so far.
- Ray
You're nto alone. It has probably been written by someone who knew what he meant :)Raymond Dunn said:even knowing the correct interpretation now, I'm not sure I understand what it said
You're telling me! These demos are full of clever tricks (like serving the TX interrupt by the RX interrupt in the UART echo demo). But without explaining how clever the code was - so everyone else can only stare at the code and wonder.Raymond Dunn said:Even the examples shown were confusing
That's a good start. Now go for error conditions, so it won't lock your master if the slave doesn't respond etc.Raymond Dunn said:I'll do some more extensive testing soon, but the slave works in the nominal cases I've tested so far.
**Attention** This is a public forum