This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hallo all,
which microcontroller of the MSP430 family supports 14-bit (or 12+2) analog-to-digital conversion???
Thanks in advance for your answer!
Hi,
you can use the MSP430 product search page to find the device you need:
http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/product_search.page
you can filter out by using the ADC parameter. There is no MSP430 has 14 bit ADC, but there are devices which has 16 bit (or more) ADC.
None.Efstratios Petrou said:which microcontroller of the MSP430 family supports 14-bit (or 12+2) analog-to-digital conversion???
The maximum SAR ADC resolution is 12 bit with up to 200ksps, the Sigma-Delta converters have 16 or even 24 bit but are only for low frequencies (few ksps with maximum resolution).
You can expand the 12 bit to 14 bit resolution by doing 16x oversampling and superimposing a sine wave of proper frequency and amplitude (=1LSB) to the signal. If you do 16 samples during one sine wave (exactly), it will average out the sine wave, but the signal itself will be lifted over the resolution threshold at different samples and therefore expand the resolution by 2 bits. Just doing 16 samples on the original signal will only apply an average but not increase resolution.
**Attention** This is a public forum