This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f2274 UART missing RX characters

Hello,

I modified "eZ430-RF2500 Wireless Sensor Monitor" Access Point firmware. Instead of sending a single char as a poll command, I send a set of characters with line ending \r\n. Sometimes I get incomplete poll command e.g. TX from Realterm client poll command [poll_t\r\n] is received [pl_t\r\n]. The actual poll is 36 char long, but you get the idea.

According to the documentation for UART (slau144.pdf), least RX error is at 12MHz and 19200baud rate which is almost 0. My configuration is as follows:

bsp_config.h

#define BSP_CONFIG_CLOCK_MHZ_SELECT    12

virtual_com_cmds.c

#elif (BSP_CONFIG_CLOCK_MHZ_SELECT == 12)

// 19200 from 12Mhz

UCA0BR0 = 0x71; 

UCA0BR1 = 0x2;

UCA0MCTL = 0;

main_AP.c

#define CMD_MAX_LEN  36

char cmdBuffer[CMD_MAX_LEN];

#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void) {
char rx = UCA0RXBUF;

memmove(cmdBuffer, cmdBuffer + 1, sizeof(cmdBuffer) - sizeof(cmdBuffer[0]));
cmdBuffer[sizeof(cmdBuffer) - 1] = rx;

if (cmdBuffer[34] == '\r' && cmdBuffer[35] == '\n') {
if (isPOLL()) {
doSomething1(); //TX data back to the client
memset(cmdBuffer, 0x0, sizeof(cmdBuffer));
} else if (isAudit()) {
doSomething2(); //TX data back to the client
memset(cmdBuffer, 0x0, sizeof(cmdBuffer));
} else { //output what's in the buffer presuming that wrong command has been sent by a client
char tmp[36];
int i;
int out = 0;
for (i = 0; i < sizeof(tmp); ++i) {
if (cmdBuffer[i] != '\0') {
tmp[out] = cmdBuffer[i];
++out;
}
}
TXString(tmp, out);

memset(cmdBuffer, 0x0, sizeof(cmdBuffer));
}
}

}

In the main loop I removed self measuring part of the temperature, Access Point is just listening for the incoming frames from End Devices.

In general it works fine, except occasional UART RX errors! 

If I am doing something silly or it could be done more efficiently, please excuse me as I am not a strong embedded C programmer.

I would appreciate any help!

Best Regards,

Rihards

  • Hi Richards,

    i think you are doing too many things in your ISR. Per default, the interrupt is disabled when you are processing an interrupt. And if you are doing too many things, this might affect the application performance. 

    I would suggest that you move most of the job into the application loop main(). The ISR could maybe only copy the received RX byte into the buffer. I would also suggest not to use the memmove() function, rather than maybe working with ring buffer and read, write indexes.

    Maybe this application report can help you also:

    http://www.ti.com/lit/an/slaa294a/slaa294a.pdf

**Attention** This is a public forum