This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am communiting with MSP430F5438A via UART using MSP430G2553. I can read and write without no error. But when i try to send 42 byte size array with MSP430F5438A, MSP430G2553 can not read the last character. Weird thing is that if i send more than 42 character, let say 50 character, MSP430G2553 can read between and including 43 and 50. I cant figure out what is the problem.
Best regards,
Recep Onur
Hi Andre,
I didnt find the reason. So instead of trying, i chose parsing data. At the end i could finish the project before. So you can close this post.
**Attention** This is a public forum