Hi,
i am using the ez430 chronos watch that has a CC430F6137 SoC. The default value of PMMCOREV is 0 according to the datasheet, however the register field has the value 3 (the highest level) at the beginning of the main function (checked with and without the debugger). I have not found anything that would change this register either in the startup code that the IAR compiler addsbefore calling the main. Therefore i wondered if the datasheet is wrong, if the chronos has a different revision of the soc or if i am missing something here.
Thanks for any hints.