Hi there,
I am programming MSP430 F5438 experimenter board using CCSv5. I use the MSP-FET430UIF to debug and power the board. I want to use ADC12 to capture the voltage using one ADC channel. However, when I switch the voltage on the channel from 3V to 0V and resume,suspend the program, the console shows MSP430: Trouble Halting Target CPU: Internal error. How to deal with this problem?
Best,
Baoqing