This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I am programming MSP430 F5438 experimenter board using CCSv5. I use the MSP-FET430UIF to debug and power the board. I want to use ADC12 to capture the voltage using one ADC channel. However, when I switch the voltage on the channel from 3V to 0V and resume,suspend the program, the console shows MSP430: Trouble Halting Target CPU: Internal error. How to deal with this problem?
Best,
Baoqing
Hi Baoqing,
I'm suffering exactly same error like you and also using same MCU, JTAG and IDE.
Did u solve this problem?
If u did, please let me know about this.
Best regards,
Woo.
**Attention** This is a public forum