This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

real time clock

Other Parts Discussed in Thread: MSP430F5438A

sir,

                  I am presently working with MSP430F5438A Experimenter board and i am using rtc example program blinking an LED for every 1 second now i want to increase time to 2 seconds how to do it?? ..and please explain about two prescale timers RT0PS  and RT1PS how they are functioning.and also help in using other interrupts while rtc interrupt.....

Awaiting for your reply,

Lokesh Bathala

  • Since the RTC is using a 32768Hz crystal as timebase, the RTX needs to count to 32768 before incrementing a second. That's the job of the prescalers. In calendar mode, the prescaler functionality is fixed and you can ignore their existence. In counte rmode, you can program the prescalers. The users guide explanation should be exhaustive.

    lokesh bathala said:
    help in using other interrupts while rtc interrupt.

    you shouldn't try (or need9 to handle any other interrutps while already handling an interrupt. Interrupt functions are fast-in fast-out. If oyu need to do any lengthy work when an interrupt is triggered, just set  aflag that the interrupt happened and handle it inside main.

    Allowign other interrupts isnide an ISR almost always leads to crashes and malfunctions that are next to untraceable. And it is almost never really necessary.

  • Why do you want to use RTC to get the interval of few seconds? you can easily use the timer for the same.

    Use RTC only when you need to use date and time, otherwise I dont see any better use of RTC time/alarm compared to timers.

**Attention** This is a public forum