This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I've looked around a bit, but I'm not finding anything on my problem...
I'm trying to program an MSP430F2131 with my launchpad and CCSv5 on Windows 7. I am connecting the VCC, TEST, RESET, and GROUND from the launchpad to the 2131. When I hit debug, I get the error message "Could not find device (or device not supported)". At first I suspected I wired it wrong, but after triple checking, trying on an F2132 (which worked fine), and trying on Linux with MSPDEBUG (same problem), I am at the end of my troubleshooting rope. Am I missing something? Do I need an update or a patch for CCS? Any help is appreciated.
-Thomas
I saw in another post that the MSP430F2131 is a 4 wire JTAG only. But I can't find the part of the datasheet that confirms this. The test pin functions for the F2132 seem the same, but I can use Spi-bi-wire just fine with that one. What's the difference between the two chips, other than RAM? And where in the datasheet does it say that the F2131 is 4 wire JTAG only?
According to MSP430 Hardware Tools User's Guide (SLAU278L.pdf – Revised December 2012) page 13, LaunchPad-G2 can be used to program F20xx, F21x2, F22xx, G2x01, G2x11, G2x21, G2x31, G2x53.
Note that F2131 is not in that list.
I see. Well that's a bummer. Thanks for the quick feedback. Guess I'll just use more F2132s and solder carefully!
Indeed, it is 4-wire JTAG only. And the datasheet of course doesn't contain information about what the device NOT has/supports. (else it would be the size of a library).Thomas Windom said:I saw in another post that the MSP430F2131 is a 4 wire JTAG only. But I can't find the part of the datasheet that confirms this.
The SBW protocol isn't mentioned as supported and there is no SBWTCK/SBWTDIO tag on the TEST/RST pins, so the SBW protocol, which the LaunchPad uses, isn't supported by this chip.
**Attention** This is a public forum