This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I am making my first steps into using IC2 on the MSP430 value line devices, using code examples supplied in the latest MSP430Ware. The examples are as follows:
MSP430G2553 has msp430g2xx3_uscib_i2c_04 - This is the Master using the USCI and should receive a single byte from the MSP430 slave.
MSP430G2432 has msp430g2xx2_usi_09 - This is the Slave using the USI and should transmit a single byte to the MSP430 master.
I have the devices connected via a breadboard, with Vcc from one board connected via 10k resistors to the SDA and SCL lines (P1.6 SDA and P1.7 SCL) as per the code example. I have given them a common ground as well, as attempting to run them off 2 computers.
So at the moment not a lot appears to happen, when I run the master, the slave reacts and jumps into the interrupt and the red LED is illuminated. But the code then jumps to the end not executing the state machine code. I suspect this is due to the process timing out as I step through the code, however if I just run both devices and press reset on the master the red LED is again illuminated (staying on) on the slave as when I stepped through the code.
I don't have access to an oscilloscope at the moment, but not 100% aufait with IC2.
So really after some advice and if I am going the wrong way about this, any suggestions appreciated.
Thanks in advance,
Ant
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430G2xx3 Demo - USCI_B0 I2C Master RX single bytes from MSP430 Slave // // Description: This demo connects two MSP430's via the I2C bus. The master // reads from the slave. This is the master code. The data from the slave // transmitter begins at 0 and increments with each transfer. The received // data is in R5 and is checked for validity. If the received data is // incorrect, the CPU is trapped and the P1.0 LED will stay on. The USCI_B0 // RX interrupt is used to know when new data has been received. // ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.2MHz // // *** to be used with "msp430g2xx3_uscib0_i2c_05.c" *** // // /|\ /|\ // MSP430G2xx3 10k 10k MSP430G2xx3 // slave | | master // ----------------- | | ----------------- // -|XIN P1.7/UCB0SDA|<-|---+->|P1.7/UCB0SDA XIN|- // | | | | | 32kHz // -|XOUT | | | XOUT|- // | P1.6/UCB0SCL|<-+----->|P1.6/UCB0SCL | // | | | P1.0|--> LED // // D. Dang // Texas Instruments Inc. // February 2011 // Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10 //****************************************************************************** #include <msp430.h> unsigned char RXData; unsigned char RXCompare; int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT P1OUT &= ~BIT0; // P1.0 = 0 P1DIR |= BIT0; // P1.0 output P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0 P1SEL2|= BIT6 + BIT7; // Assign I2C pins to USCI_B0 UCB0CTL1 |= UCSWRST; // Enable SW reset UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz UCB0BR1 = 0; UCB0I2CSA = 0x048; // Slave Address is 048h UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation IE2 |= UCB0RXIE; // Enable RX interrupt RXCompare = 0; // Used to check incoming data while (1) { while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent UCB0CTL1 |= UCTXSTT; // I2C start condition while (UCB0CTL1 & UCTXSTT); // Start condition sent? UCB0CTL1 |= UCTXSTP; // I2C stop condition __bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts if (RXData != RXCompare) // Trap CPU if wrong { P1OUT |= BIT0; // P1.0 = 1 while (1); // Trap CPU } RXCompare++; // Increment correct RX value } } // USCI_B0 Data ISR #pragma vector = USCIAB0TX_VECTOR __interrupt void USCIAB0TX_ISR(void) { RXData = UCB0RXBUF; // Get RX data __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 }
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430G2xx2 Demo - I2C Slave Transmitter, single byte // // Description: I2C Slave communicates with I2C Master using // the USI. Slave data is sent and increments from 0x00 with each transmitted // byte which is verified by the Master. // LED off for address or data Ack; LED on for address or data NAck. // ACLK = n/a, MCLK = SMCLK = Calibrated 1MHz // // ***THIS IS THE SLAVE CODE*** // // Slave Master // (MSP430G2xx2_usi_06.c) // MSP430G2xx2 MSP430G2xx2 // ----------------- ----------------- // /|\| XIN|- /|\| XIN|- // | | | | | | // --|RST XOUT|- --|RST XOUT|- // | | | | // LED <-|P1.0 | | | // | | | P1.0|-> LED // | SDA/P1.7|------->|P1.7/SDA | // | SCL/P1.6|<-------|P1.6/SCL | // // Note: internal pull-ups are used in this example for SDA & SCL // // D. Dang // Texas Instruments Inc. // December 2010 // Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10 //****************************************************************************** #include <msp430.h> char SLV_Data = 248; // Variable for transmitted data char SLV_Addr = 0x90; // Address is 0x48<<1 for R/W int I2C_State = 0; // State variable int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog if (CALBC1_1MHZ==0xFF) // If calibration constants erased { while(1); // do not load, trap CPU!! } DCOCTL = 0; // Select lowest DCOx and MODx settings BCSCTL1 = CALBC1_1MHZ; // Set DCO DCOCTL = CALDCO_1MHZ; P1OUT = 0xC0; // P1.6 & P1.7 Pullups P1REN |= 0xC0; // P1.6 & P1.7 Pullups P1DIR = 0xFF; // Unused pins as outputs P2OUT = 0; P2DIR = 0xFF; USICTL0 = USIPE6+USIPE7+USISWRST; // Port & USI mode setup USICTL1 = USII2C+USIIE+USISTTIE; // Enable I2C mode & USI interrupts USICKCTL = USICKPL; // Setup clock polarity USICNT |= USIIFGCC; // Disable automatic clear control USICTL0 &= ~USISWRST; // Enable USI USICTL1 &= ~USIIFG; // Clear pending flag _EINT(); while(1) { LPM0; // CPU off, await USI interrupt _NOP(); // Used for IAR } } //****************************************************** // USI interrupt service routine //****************************************************** #pragma vector = USI_VECTOR __interrupt void USI_TXRX (void) { if (USICTL1 & USISTTIFG) // Start entry? { P1OUT |= 0x01; // LED on: Sequence start I2C_State = 2; // Enter 1st state on start } switch(I2C_State) { case 0: //Idle, should not get here break; case 2: //RX Address USICNT = (USICNT & 0xE0) + 0x08; // Bit counter = 8, RX Address USICTL1 &= ~USISTTIFG; // Clear start flag I2C_State = 4; // Go to next state: check address break; case 4: // Process Address and send (N)Ack if (USISRL & 0x01) // If read... SLV_Addr++; // Save R/W bit USICTL0 |= USIOE; // SDA = output if (USISRL == SLV_Addr) // Address match? { USISRL = 0x00; // Send Ack P1OUT &= ~0x01; // LED off I2C_State = 8; // Go to next state: TX data } else { USISRL = 0xFF; // Send NAck P1OUT |= 0x01; // LED on: error I2C_State = 6; // Go to next state: prep for next Start } USICNT |= 0x01; // Bit counter = 1, send (N)Ack bit break; case 6: // Prep for Start condition USICTL0 &= ~USIOE; // SDA = input SLV_Addr = 0x90; // Reset slave address I2C_State = 0; // Reset state machine break; case 8: // Send Data byte USICTL0 |= USIOE; // SDA = output USISRL = SLV_Data; // Send data byte USICNT |= 0x08; // Bit counter = 8, TX data I2C_State = 10; // Go to next state: receive (N)Ack break; case 10:// Receive Data (N)Ack USICTL0 &= ~USIOE; // SDA = input USICNT |= 0x01; // Bit counter = 1, receive (N)Ack I2C_State = 12; // Go to next state: check (N)Ack break; case 12:// Process Data Ack/NAck if (USISRL & 0x01) // If Nack received... { P1OUT |= 0x01; // LED on: error } else // Ack received { P1OUT &= ~0x01; // LED off SLV_Data++; // Increment Slave data } // Prep for Start condition USICTL0 &= ~USIOE; // SDA = input SLV_Addr = 0x90; // Reset slave address I2C_State = 0; // Reset state machine break; } USICTL1 &= ~USIIFG; // Clear pending flags }
Brian,
Thanks for confirming that, I will try a higher value for the pullups as well.
Not sure if you have had a chance to look at the code, but is there anyway to slow the process down so I can try and identify what is happen?
Regards,
Ant
Really the best way to see what's happening at the physical layer is to probe the lines with an oscilloscope and decode the I2C transaction to make sure it looks correct.
Barring that, another option is to connect some LEDs to unused port pins and turn them on/off at specific points in the program, but even then they might be too fast to get a good understanding.
Being used to digital electronics, I tend to do high-value pullups as well. But on I2C, there often is a rather high line capacitance and mroe than just one input. With 47k pullup you won't see nice signals when going to 400kBd bus speed.Brian Boorman said:although I tend to use 47K-ish pullups
After all, when the bus is in idle state, the pullup doesn't draw any current, no matter how low it is.
Hi Jens,
Thanks for the information I have read on other sites 33k is a good half way value to consider. I am still still struggling to see what is happening though with the TI code, and wondering if there is an easy way to amend the code and implement a loop in the hand shaking and data transfer, so that the Master requests the information continuously from the Slave. Therefore the Slave should react and send the data back and I should be able to see the variables change with a breakpoint and refresh values in Code Composer.
Best regards,
Ant
It really depends on clock speed, line length and number of peers.Ant Scranney said:Thanks for the information I have read on other sites 33k is a good half way value to consider.
As for the application, many slaves offer a' new data ready' signal which is checked by the master and then data is read.
You may as well initiate a transfer and continuously read data, while the slave updates it when available. But this will waste quite some CPU power and also keeps the bus busy.
However, with the USCI, you cannot simply stop polling data and continue later, as the USCI uses double-buffering, continuing to read data while you haven't even read the last one. So stopping a read transfer by jsut holding the clock, and continuing later, is a bit difficult on I2C.
**Attention** This is a public forum