Other Parts Discussed in Thread: MSP430FG4618
Hello everyone,
I am using IAR embedded workbench for programming MSP430FG4618/F2013 and TI USB-FET to program the same. I was able to program the MCU yest and the debugger was working fine. Now it shows an error message and I am not able to dump the code on the device.
The emulator message shown is as follows.
Fatal error : failed to initialize
Check if hardware is connected.
Check if drivers are installed.
Try to restart the computer.
Tools using the parallel port are not supported on vista. ( I m using windows XP)
Session aborted.
I have verified all of the above, but still I am having the same problem. Any suggestions..??????