This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I am using MSP-EXP430F5438 board on windows 7.The drivers seem to be installed correctly as seen below:
Yet I am unable to open a HyperTerminal (manually installed on windows 7) on the COM 1 port...
Did anyone seen this problem? How to overcome it?
Regards
Igor
Igor Shvorin said:Yet I am unable to open a HyperTerminal (manually installed on windows 7) on the COM 1 port...
Did anyone seen this problem? How to overcome it?
Never had this problem. But can you be more specific? What is the error message you are getting?
Hi
I am not getting any error.The HT(HyperTerminal) does not show a COM1 in a list of available ports and thus I am not able to open a HyperTerminal on the MSP port for UART communication...
Okay.
I am guessing here that you are using the HT App for Windows 7.
We had experience other problems with this app.
I suggest you use TeraTerm (http://ttssh2.sourceforge.jp/index.html.en)
Its a freeware. After you have installed the board software (which you did), I hope you have restarted the PC.
Also if you dont get COM1 in the first go in TeraTerm, wait for 15 seconds and try again
Keep posted
Cheers
Hi Thanks for good will to help, but it seems not working once again.
Another piece of information is that I am running Win7 on MAC (via Parallels). Any other idea?
Okay. That information is very essential
I do not have any experience with Parallels, but I suppose its similar to VirtualBox.
So you need to find something like Serial Port Settings in Parallels configuration.
As you are connecting via USB, it may be useful to add a new USB device in Parallels.
There are settings in VirtualBox to add USB device in virtual machine. I think they should be there for Parallels too
Hi
Thanks a lot for help...
I am able to map it to parallels otherwise the driver will nto be installed :-)
I assume that the fact that Win 7 is detecting the MSP board and installs a required driver means that the USB port is mapped to Win.
Any other ides?
Thanks for information...
May be TI guys have a bit easier way to resolve an issue?
It is a common problem that soem badly designed mouse driver or smartphone-syncing app will hijack the port and block it for any other applicaiton.Debasish Banerjee said:Or is it exclusively being used by an another application? Hope you won't mind.
BTW, there was a years newer version of HyperTerm available for free privat euse years ago, on which several bugs were fixed (inclusding the backscroll buffer quirks). However, ht emanufacturer doesn't offer it anymore.
Microsoft kept delivering a stone-age version on XP (and Win7?), years after the newer one was out.
I still use it (sometimes, I have 6 terminal windows open simultaneously, and all remember their positions and settings by the link on my desktop - somehting none of the replacements does) even though I also have putty (mostly for VPN tunneling) and some others.
**Attention** This is a public forum