This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI,
I have a question regarding the MSP430 USB Firmware Upgrade Example - was there a BSL_UART_GUI 'namespace' done vs. just the USB version?
The code to support either interface is there - but of course there is not a way to select a serial port for the UART, etc. in any of the GUI graphics (yet).
The BSL_430_DLL of course supports either interface.
It would appear at one time this program may have had a native UART GUI - is that true? If so, can that be posted?
If not - are there any plans to have it? Would be nice to support either interface with the GUI based version of the BSL code.
I have modified the source so that the UART BSL invokes - so it does work - right now I have to 'hard code' so to speak the COM port setting.
Thanks,
johnw
**Attention** This is a public forum