Hi guys,
I am working on a base station that receives data from an end device using simpliciTI. The information will be handled to a PC via USB. So far I have used the MSP430FG4618 experimenter's board as end device along with the CC2500EMK. The original base station is another MSP430FG4618 experimenter's board + CC2500EMK. The data is sent properly and now want to dump it into a virtual COM port on a PC.
I am trying to implement the base station on the MSP430f5529 USB Experimenter's Board to take advantage of the USB capabilities of the F5529. I want to have SimpliciTI (also using the CC2500EMK) on the MSP430f5529 USB Experimenter's Board to communicate with my end device but it seems that the stack is not available for this board (at least on SimpliciTI V1.1.1).
Can you tell me what do I need to modify on the BSP folder to get simpliciTI working on the MSP430f5529 USB Experimenter's Board?
Thanks,
Efrain