Hi I'm a new user
I want to know if there is a useful MSP430 mictocontrollers book
with many C Code examples.
Anthony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi I'm a new user
I want to know if there is a useful MSP430 mictocontrollers book
with many C Code examples.
Anthony
Anthony Pontikakis said:I want to know if there is a useful MSP430 mictocontrollers book
with many C Code examples.
How helpful are these online resources?
Here's a book
TITLE: Microcontroller Programming and Interfacing: Texas Instruments Msp430
by Pack, Daniel J. And Barrett, Steven
ISBN: 1608-45713-3
ISBN 13: 978-1608-45713-7
Publisher: Morgan & Claypool Publishers
Publish Date: 2011-06-30
Binding: Paperback
List Price: USD 50.00
"useful" depends on what you want to do. If you don't know anything and want to learn something, any book is useful.Anthony Pontikakis said:I want to know if there is a useful MSP430 mictocontrollers book
I doubt that any book contains significantly more information than one could get or deduct from those two. There might be ideas, explanations etc. But (writing on an MSP book myself) I know that all of this could be derived from these two resources by a skilled engineer.
I have found the book below very useful:
MSP430 Microcontroller Basics by John H. Davies
The book describes the concepts and the peripherals very well and includes many examples. I highly recommed it.
Jens-Michael Gross said:Starting with the users guide (a 'book' most people seem to avoid like the devil avoids holy water) and the device datasheets (another one that is regularly ignored)
I doubt that any book contains significantly more information than one could get or deduct from those two.
Does automobile service manual contains any driving instructions? Here I mean that hardware guide does not explain applications where particular hardware can be used for..
It does - as far as using the features of the car is concerned. It does not, however, include instructions on how to comply with the local rules of public traffic.Ilmars said:Does automobile service manual contains any driving instructions?
Of course the guide doesn't explain applications. That would be half-way to providing a complete solution (like the 'I bought this MSP, now give me the code for my project' forum posts).
However, the original post did begin with "I'm new', so the first thing someone should read are the users guides. Those who start with a collection of half-baked example codes won't ever get anywhere but into this forum, calling for help (as they don't really understand what their sample codes are doing).
I've seen books full of nice C/C++ programming tricks. Without ever looking into K&R or such, you'll never understand how they work, or go beyond simply reproducing them. Same for hardware (of any kind).
Start with the general and then develop the specific. And you don't need any sample books.
Jens-Michael Gross said:And you don't need any sample books.
Anyway - before deciding to not have any sample books, please check this one:
MSP430 Family
Mixed-Signal Microcontroller Application Reports
http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=slaa024
Nice, but outdated by far. It is about the discontinued 3x family MSPs and much of its content doesn't fit to the currently available MSPs at all.Ilmars said:Anyway - before deciding to not have any sample books, please check this one:
**Attention** This is a public forum