This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a problem locating the third USCI B I²C Port (USCI_B0) (MSP430F6659IPZ).
The other two are located at P9.6, P9.5 and P8.6, P8.5 due to the datasheet. Or is there no connection to the USCI_B0 possible in this package?
Best regards
Look at Table 2 on Page 11 of the datasheet.
The USCI_Bx and USCI_Ax functions are on the Port 2 P2MAPx port mapping pins.
Also make sure to read the User's Guide on correct operation of the port mapping function.
**Attention** This is a public forum