Hello everyone,
I am having trouble trying to get MSP-FET430UIF recognising and talking to an evaluation board that has a MSP430F5528 on it. It is powered by a small Li-Polymer battery followed by a 3V regulator and has a 14-ping JTAG header. The FET has V3 firmware on it. However, when I try to connect to the board using MSP430Flasher (both on Windows 7 and Linux) I keep getting "Could not set device Vcc" error. However, I have checked that pin-4 of the JTAG header is connected to regulator output and has 3V on it with the FET cable connected to it. I have also tried to power the board by disconnecting the battery and shorting out pin-2 and pin-4 of the JTAG connector but I still get the same error.
It appears that others have also had similar problems and some has suggested to downgrade to V2 and then upgrade to V3 firmware. I have installed CCS 5 but cannot find a way of doing that. Any suggestions or help will be really appreciated.