This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
CCS v7.1.0.00016
Windows 10 Pro
MSP-FET SN:180300301
I just bought the new FET. We have used the old MSP-FETU430IF for probably 8 years or so. The old FET works still and the new FET works on a colleagues machine running windows 7 with the same version of CCS. Problem exists whether the target board is connected or not. Using the same JTAG connection for the old and new FET.
New FET works with UniFlash on the both my machine and my colleagues machine. UniFlash did update the firmware in the FET on the first use.
I have uninstalled and reinstalled CCS. We don't want to upgrade to a new version at this point in our development cycle. We can use the old FETs in the meantime.
Any help or tips for troubleshooting would be greatly appreciated.
-shawn
1. No, CCS 7.1 did not update the firmware.
2. MSP Flasher version 1.3.18 does work with the new FET.
MSP Flasher updated the firmware in the FET, but it and UniFlash (v 4.2.0.1490) are requiring different versions and taking turns trying to update it. I thought they were both the most recent versions. CCS doesn't seem to care which version the FET has.
I looked at the log.txt files for both the firmware update and flash write with MSP Flasher and see nothing of interest.
-s
OK, understood. I will look at my colleague's machine and see what version his dll is. It seems odd that we would have exactly the same version of CCS and a different version dll.
We will upgrade our development suite at the first opportunity.
Thank you.
s
We have elected to upgrade to CCS v8.1. The new MSP-FET is functioning properly now. Thanks for the help.
**Attention** This is a public forum