Part Number: MSP-FET
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi,
any help will be highly appreciated. I am an HW engineer and have to deal with updating a test fixture which among others can program an MSP430.
It uses an MSP-FET USB programmer working fine wih the MSPFlasher_1.3.8 in a production setup.
Then by mistake I temporarily applied 12V on the test board on the Vcc pin, instead of 3.3V. This rendered the board dead and the original programmer was affected too.
So I get a new MSP-FET from Digikey, a new board to be programmed, and now cannot get past this error:
"C:\Users\pr34x\Desktop>cd \ti\MSPFlasher_1.3.8\
C:\TI\MSPFlasher_1.3.8>MSP430Flasher.exe -n MSP430G2x55 -w "prx_pmic_v17.hex" -v
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.8 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Found USB FET @ COM8 <- Selected
* Initializing interface @ COM8...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...
# Exit: 44
# ERROR: Could not set device Vcc
* Powering down...done
* Disconnecting from device...
* ----------------------------------------------------------------------------
* ERROR on close: Could not set device Vcc
* ----------------------------------------------------------------------------
*/
C:\TI\MSPFlasher_1.3.8>pause
Press any key to continue . . .
"
Any ideas?
Thank you