Part Number: MSP-EXP430FR2433
Other Parts Discussed in Thread: UNIFLASH, EK-TM4C129EXL,
Tool/software: Code Composer Studio
Hi,
I'm having an issue trying to program a MSP43FR2433 Launchpad with CCS 8.3.0. It keeps trying to update the firmware on the board but bombs out setting the VCC. I've tried with MSPFlasher and UniFlash and in all cases it fails for "ERROR on close: Could not set device Vcc".
I've used this board before so am I am not sure why I am seeing this issue now.
Also, I have looked at the previous posts and have not found a solution for this.
This is the output from MSPFlasher.
C:\ti\MSPFlasher_1.3.19>MSP430Flasher.exe -i DTECT * -----/|-------------------------------------------------------------------- * * / |__ * * /_ / MSP Flasher v1.3.19 * * | / * * -----|/-------------------------------------------------------------------- * * * Evaluating triggers... * Invalid argument for -i trigger. Default used (USB). * Checking for available FET debuggers: * Found USB FET @ COM9 <- Selected * Initializing interface @ COM9...done * Checking firmware compatibility: * The firmware of your FET is outdated. - Would you like to update it? (Y/N): y ********************************************************* * * Initializing Update Bootloader. * Programming new firmware: * |||||||||||||||||||||||||||||||||||||||||||||||||| 100% * Update was successfully finished. * ********************************************************* * Exit Update Bootlader and reboot firmware. * FET firmware is up to date. * Reading FW version...done * Setting VCC to 3000 mV... # Exit: 44 # ERROR: Could not set device Vcc * Powering down...done * Disconnecting from device... * ---------------------------------------------------------------------------- * ERROR on close: Could not set device Vcc * ---------------------------------------------------------------------------- */ C:\ti\MSPFlasher_1.3.19>