This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
One customer wants to use MSP430F55xx USB BSL and UART BSL code for MSP430F563x directly, before they already used USB BSL and UART BSL successfully on MSP430F5526. In the latest BSL source code, SLAA450 1_00_06_00, it only have the USB and UART BSL source code for MSP430F5526, can we use it directly for MSP430F5635? If not, what we need to modify for the porting? Thanks.
I have compared their USB pin map, UART pin map and BSL memory map, they are all the same. However, the start address of main memory is different.
BR,
Lina
**Attention** This is a public forum