This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2955 SPI communication

Hi!

I am trying to communicate between two MSP430G2955 using the SPI(Master/slave) protocol. Currently, I am using the example codes provided in the resource explorer. However, I am not able to see any data on the logic analyzer. I tried different combinations for UCCKPL and UCCKPH, but still no success. Could someone point out the possible errors.

The hardware connections are as follows:

MASTER      SLAVE
MOSI--->MISO

MISO--->MOSI

CLOCK out-->CLOCK in

Chip select-->RST/NMI

Any leads would be appreciated.

Thanks

**Attention** This is a public forum