This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Champs,
Is anyone aware of an updated msp430f5217.h header file? The version I have is 1.1; it came with IAR6.50.1 but I noticed the CCSv6 also has the same version included. This file doesn't have the Port7 defines in it. I added those so I'm up and running, but not real clear to me if I'm missing anything else I'll later need.
Hi radar,
Thanks for reporting this, and I can confirm this appears to be missing from the F5217 header. I can see that in F5229 (superset part in the same family) header file it says #define __MSP430_HEADER_VERSION__ 1153 Which is the same version number I see in the F5217 header file, but the F5229 correctly has the Port7 defines while F5217 does not.
I will file this as a bug to get fixed in the next release.
Regards,
Katie
**Attention** This is a public forum