This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Few days ago, i wanted to power my breadboard circuit from the Launchpad. From that day on, whenever i plug launchpad on USB with MSP430G2553 mcu, red and green led stay very dimmed and when i try to program the chip (either with IAR or with Energia) it says that device cannot be found. On Windows device manager, i can see the launchpad getting assigned to COM port. If i switch the mcu with G2452, everything works fine. Does anyone have any idea why this happens? Should i replace my launchpad with a new one or can it be fixed?
Thanks in advance.
You could also try the following steps.
(1) Power down your PC.
(2) Plug G2553 to the socket on the LP board.
(3) Check all the jumpers on the LP board.
(4) Plug LP to a USB port.
(5) Power up the PC.
If this still does not work. You may try a different USB on your PC. But you must use steps (1), (4), and (5) again in that order.
**Attention** This is a public forum