This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My application on MSP430F5310 showed weird behavior at the customer (stopped running after a few minutes). After quite some fiddling around, I suppose that the problem was due to insufficient stack size. The application makes heavy use of the stack, so the default setting might have been too small. Now the setting is at 1.5 kB stack, so far everything looks fine.
Does someone have a suggestion how to detect a stack overrun at runtime? Cyclically checking the stack pointer? Setting and checking a bit pattern just below the stack? Any other wonderful idea I did not come across?
Max
To easily check stack-use add the following lines to your program, immediately at the begin of main and just after stopping the watchdog. Let the program run a while and stop it, check the stack contents with the memory-browser, if all A5 are gone you can be sure you have a stack overflow and needs to increase stack-size.
extern unsigned int _stack; extern unsigned int __STACK_END; unsigned int* p; p = &_stack; while (p < (&__STACK_END -3)) { *p = 0xA5A5; p++; }
That’s correct. You can verify this in the “<configuration>\<project>.map” output file.
**Attention** This is a public forum