This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have constructed the demo in slaa600a of the msp430boot with the Launchpad and the g2553 uC .
I have problems with 6.3 number 2, where I have to convert the output of the applications crc and implement it in the hostprogramm. I do not know where to put the output c file in the host project, since when I simply paste it in the program folder of MSP430BootHost, the program does not built/ has errors.
I used the bat programm, since I use 2 launchpads like in the demo
I would be happy if you could help me with this.
Thanks,
**Attention** This is a public forum