This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm facing a problem using the MSP430F5438A I2C peripheral in transmiter slave mode. Receiver slave mode works perfectly.
The master issues a Read request (slave address = 0x10) and tries to read 3 bytes. At the slave (MSP430) the byte 0x0C is always reloaded whenever the interrupt with origin in UCTXIFG is activated.
I'm using 7bit addressing, no multi-master, 12k pull ups.
The results:
Address byte -> OK
First byte -> OK
Second byte -> The MSP is one clock desynchronized. Due to that, it fails to read the ACK send by the master which is issued one clock later.
Third byte -> Aborted in the MSP, the master reads it as 0xFF
Please see the picture. In this example, the clock is extremely slow to avoid any high speed issues.
Am I doing something wrong?
Thank you
I realize this is an old thread, but I just hit the same problem.
In my example of this the MSP430 is the bus master, and has two peripherals attached to it. One of the peripherals works perfectly, and the other has the first byte of the i2c message shifted left one bit. The chip address is fine, but the register address is shifted.
What did you end up doing? Was it resolved?
Thanks!!
Hello,
As far as I remember, Jens-Michael Gross was right about clock stretching. In my case, the MSP430 was in slave mode and trying to stretch the CLK while loading the next octet. However, the master (an FTDI chip) did not support clock stretching and was creating this kind of problems. I think I tried to optimize the code and avoid having other interrupts which may delay the loading of the next octet to TXBUF.
Best regards,
Mário
**Attention** This is a public forum