Other Parts Discussed in Thread: ENERGIA, MSP430WARE
I was trying some of the msp432 C device samples with CCS on ubuntu 14.04. Some work as expected however I'm having a problem with the sample
msp432p401_pcm_09 - device operation at 48MHz with DC-DC Regulator
It seems like it should work as the launchpad seems to have the proper inductor. I've tried this in an up to date CCS 6.1.0 on 32 bit ubuntu and with the cloud based dev.ti.com site. Both are able to program the board however the code fails and ends up in the error routine and just sits there blinking at me without setting the PCM values or the 48 MHz clock.
Has anyone else tried this sample on an msp432 launchpad? Did it work for you?
-rick