This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
where can I get the USB drivers for the MSP432 Launchpad?
Im running CCS6.1.0 under WINXP, if I connect the board, the hardware installation routine starts and ask for XDS110 USB driver.
If I search in the folder "ti", I cant find it.
Thanks.
Stefan
OK, then maybe it is because Windows XP? I don't know - I remember something with a missing driver, but I'm not 100% sure. You can try these drivers:
Dennis
Hi Dennis,
I had the same problem on Windows 7 professional. Your link solves the problem. Thank you
John
**Attention** This is a public forum