This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Hardware Multiplier?

Other Parts Discussed in Thread: MSP430FG4618

Hi, i'll use hardware multiplier, signed multiply and accumulate. I saved data in msp430fg4618 flash memory. I want to ask how can i read data from flash memory? I mean my data located at flash 0x7000 address. If i use OP2 = 0x7000, multiplier use 0x7000 value not my data's value. I want to use my data's value in OP2 not address value. How can i do that?

Thanks.

  • Hi Ferhat,

    Shouldnt you be using pointer to the flash address to read the value at the address and not the address itself?

    Something like (int*)(0x7000) should give you the value at the Flash address, if i am not wrong.

    Regards,

    Sid

  • Hi sid, i tried that but there is a compiler error (IAR), it says ' Error[Pe513]: a value of type "int *" cannot be assigned to an entity of type "unsigned short"  '.

  • Hi Ferhat,

    Have you tried replacing int* with (unsigned short*)? Since you are using a 16-bit microcontroller.

    Regards,

    Sid

  • Yes, i tried that too but result is same, Error[Pe513]: a value of type "unsigned short *" cannot be assigned to an entity of type "unsigned short" .

  • OP2 is a register in the hardware multiplier that needs to be written with the value of the operand, not the address of the operand.  If your operand physically resides at address 0x7000, then the following should be used.

    unsigned short * operand2 = 0x7000 ;

    OP2 = *operand2 ;

  • I tried that but it gave similar error, Error[Pe144]: a value of type "int" cannot be used to initialize an entity of type "unsigned short *". So i tried this,

    unsigned int * operand2 = 0x7000;

    OP2 = *operand2;

    and compiler says, Error[Pe144]: a value of type "int" cannot be used to initialize an entity of type "unsigned int *".

    I tried int * operand2, compiler gave similar error again.

  • Sorry, my fault.  I was a little quick on the trigger.

    unsigned int * operand2 ;

     

    operand2 = (unsigned int *)0x7000 ;

    OP2 = *operand2 ;

  • Hi Ferhat,

    Missed the * sign in my post.

    *(unsigned short *)(0x7000) or *(int *)(0x7000) should give you the value at corresponding flash address.

    Regards,

    Sid

  • Thanks for help.

    Ferhat

**Attention** This is a public forum