This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, i'll use hardware multiplier, signed multiply and accumulate. I saved data in msp430fg4618 flash memory. I want to ask how can i read data from flash memory? I mean my data located at flash 0x7000 address. If i use OP2 = 0x7000, multiplier use 0x7000 value not my data's value. I want to use my data's value in OP2 not address value. How can i do that?
Thanks.
OP2 is a register in the hardware multiplier that needs to be written with the value of the operand, not the address of the operand. If your operand physically resides at address 0x7000, then the following should be used.
unsigned short * operand2 = 0x7000 ;
OP2 = *operand2 ;
I tried that but it gave similar error, Error[Pe144]: a value of type "int" cannot be used to initialize an entity of type "unsigned short *". So i tried this,
unsigned int * operand2 = 0x7000;
OP2 = *operand2;
and compiler says, Error[Pe144]: a value of type "int" cannot be used to initialize an entity of type "unsigned int *".
I tried int * operand2, compiler gave similar error again.
Sorry, my fault. I was a little quick on the trigger.
unsigned int * operand2 ;
operand2 = (unsigned int *)0x7000 ;
OP2 = *operand2 ;
Hi Ferhat,
Missed the * sign in my post.
*(unsigned short *)(0x7000) or *(int *)(0x7000) should give you the value at corresponding flash address.
Regards,
Sid
**Attention** This is a public forum